Cannot find Oncam camera on network

Issue

Can't find Oncam camera on the network even when using a device utility

Product Line

Pelco Cameras, Pelco Video Management

Environment

Oncam cameras when on any VMS or network

Cause

The Oncam cameras do not roll to the next higher number if you use it's static IP address. If you have more than one at a time they would both come up with the default address of 192.168.0.200 and there would be a network IP address conflict. This would cause one or more not to be seen on the network

Resolution

Use a DHCP server or only put one camera on the network at a time and then manually change the address