Access to Linux in the AS has been restricted in StruxureWare Building Operation 1.5, and is not supported

Issue

When trying to login to Linux console via Device Administrator the console display says the Admin account is locked out.  

Product Line

SmartStruxure Solution

Environment

  • StruxureWare Building Operation 1.5
  • Linux
  • WinSCP

Cause

Linux cannot be accessed via Device Manager Console or utilities like WinSCP.

Resolution

Access to Linux in the AS no longer available in StruxureWare Building Operation 1.5