POE1XT not powering up IP camera?

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

NOTICE

POTENTIAL FOR DATA LOSS.
The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure, please contact Product Support Services prior to attempting the procedure below.

Issue

No power out on POE1XT.

Product Line

Pelco Transmission & Power

Environment

  • POE1XT

Cause

No power output due to incorrect jumper setting. 

Resolution

Move the jumper on this power supply to the right according to the picture shown.