Sarix TI model Thermal imaging color gradient Preset command manipulation.


  • How do I get the Sarix TI camera to change to a different color refernece for hot/cold levels?
  • How do I get the Sarix TI to change to rainbow effect for video?
  • How do I use the Preset commands to change the Sarix TI between the color references for hot/cold areas?
  • Which Preset do I need to change to certain color ranges in the Sarix TI?
  • Can I use the Preset command sets to change the color temperatures inside the Sarix TI across the Network?

Product Line

Pelco Cameras


Sarix TI models: TI206; TI635; TI650, TI6100


Correct reference to the Sarix TI's manual has not been made in order to understand the Preset command sets and how they are to be sent to the Sarix TI units.


In order to get the Sarix TI to change, manually, into different color temperature ranges is to use the following Preset commands from a KBD300A conncted to the two [Green/White (RX+) and Green (RX-)]:

Sarix TI Preset command reference from Page #58 of the 1317M-C IO manual.

How to connect a KBD300A in Direct mode reference: LL#9921.