Profile G compliant Sarix IME and IMP camera use of the SD Card.

Issue

  • What SD card can I use inside the new Profile G Sarix cameras?
  • In order to use Profile G, what SD card do I have to use?
  • Do the Sarix Profile G compliant cameras now let use larger SD cards?
  • Do the newer IMP and IME lines of cameras have better use of the SD cards

Product Line

Pelco Cameras

Environment

Sarix IME and IMP cameras on version 2.1.

Cause

Pre-sales inquiries about Enhanced and Professional series of the new Sarix lines of cameras.

Resolution

The newer version 2.1 for the IME (Enhanced) and IMP (Professional) lines of cameras allows for ONVIF Profile "G" Edge recording at the camera through the SD card, 32 GB SanDisk Extreme® PLUS microSDHC™ UHS-I card. This is an extremely specific spec on the SD card to use and thereore NO other model of SD card is guaranteed to provide as much recording and utilization through Profile G. However, other models of SD cards are fine to use, but, when Profile G is concerned, the above named SD card MUST be used.