IPCT01 not charging

Issue

When charging IPCT01,  blue light indicator does not come on. 

Product Line

Other, Pelco Transmission & Power

Environment

IPCT01

Cause

When powered up blue light does not come on.

Resolution

There are 2 reasons why this light is not on.

1. The battery is fully charged

2. If the battery terminals are dirty, battery performance will decrease. Clean the terminals with a cotton swab