Does the DS1000 support multiple recording rates for analog cameras?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Does the DS1000 support multiple recording rates for analog cameras?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry
  • DS1000

Cause

Request to configure two seperate recording rates for an analog camera connected to a DS1000 unit.

Resolution

The DS1000 has the limitation that mutliple recording rates can not be adjusted within DSAdmin, preventing the ability of using multiple record rates.

The DS1000 can only use the single recording rate that is adjusted from the video input device. All viewable rates will then match the rate configured.