Installing DS ControlPoint version 7.7.309 on Windows XP workstation fails.

Issue

When attempting to install DS ControlPoint version 7.7.309 on Windows XP workstation fails due to failure to install the required .NET Framework 4.5.1 which is not supported on this operating system.

Product Line

Pelco Video Management

Environment

  • DS
  • ControlPoint
  • Windows XP
  • Windows 2000
  • Server 2003

Cause

Digital Sentry DS ControlPoint is designed for workstations running Microsoft® Windows® Server®2008, Windows Vista®, or Windows 7. Microsoft no longer supports Windows 2000; therefore,DS ControlPoint is no longer supported by Pelco on the Windows 2000 platform.

Resolution

Install DS ControlPoint version 7.6.32.  Download ControlPoint 7.6.32