BU4 Series Power Requirements

Issue

BU4 Series Power Consumption

Product Line

Pelco Cameras, Pelco Transmission & Power

Environment

BU4 Series

Cause

Power Consumption

Resolution

  • BU4 Series ONLY support 12 VDC +10%, 60Hz
  • Power Consumption: 3 W (IR on, without heater) and 8 W (IR on, with heater on)
  • Click HERE for the Specification Sheet
  • Click HERE for Altronix website view of power supplies. Go to Products/Power Supplies and use the Product Finder selection guide (image)
    Output Type: DC; Version: Outdoor; Input Voltage: 115vac; Number of Outputs: 1; Output Protection: Fuse; Fire Alarm: No.

Note: Pelco doesn't offer 12 VDC power supply at the meantime.