Why does it look different in Webstation and Workstation when forcing a value?

Issue

When forcing a value from Webstation there is no description from the point and the whole path is printed, it is hard to read and doesn't look nice.
 

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation 1.5

Cause

It looks different because both clients have been gradually improved over time.

Resolution

The Edit value controls in WebStation is being rewritten for the non-Java viewer of graphics and looks more like WorkStation and shows Description.