How to set a park time for spectra or esprit PTZ using the KBD300A, KBD200, and KBD4000

Issue

How do i turn on the park time for spectra or esprit using the KBD300A

Product Line

Pelco Cameras

Environment

  • Spectra series PTZ
  • Esprit series

Cause

  • Editing Park Time of the Spectra or Esprit Series requires entry to the 95 Preset Menu from your control system
  • Set park time minutes to enable park action

Resolution

Spectra series and ES40/ES41 series follow instructions below.

  1. Tap 95 then press and hold Preset. Main menu appears.
  2. Toggle down to "Dome Settings" and tap Open
  3. Toggle down to "Motion" and tap Open
  4. Toggle down to "Park Time" and tap Open
  5. Toggle down to set the minutes from 1 to 720
  6. Tap Open. Park time minutes is now set to the minutes that was set
  7. Toggle down to "Park Action" and tap Open to set the park action to the desired action ( example preset 1)
  8. Tap Open. Park action is now set.
  9. Toggle down to "Exit" and tap Open. Exit from main menu.

 

ES30/31 Series use the following steps.

  1. Tap 95 then press and hold Preset. Main menu appears.
  2. Toggle down to "Other" and tap Open
  3. Toggle down to "Park Time Minutes" and tap Open
  4. Toggle down to set the minutes from 1 to 720
  5. Tap Open. Park time minutes is now set to the minutes that was set
  6. Esprit will park to preset 1 location set ( Note: Preset 1 must be programmed for the Esprit to park.)
  7. Tap Open. Park is now set.
  8. Toggle down to "Exit" and tap Open. Exit from main menu.