Comparison Between DSSRV, DSSRV2, DSSRV2-RD

Issue

Customers would like to know the differences between hardware platforms.

Product Line

Pelco Video Management

Environment

Digital Sentry
DSSRV
DSSRV2
DSSRV2-RD

Cause

Due to parts in the original DSSRV going End Of Life, a new hardware platform was created.

Resolution

 

 
 

DSSRV

DSSRV2

DSSRV2-RAID

System Throughput

280Mbps

300Mbps

350Mbps

OS Drive

Shared with storage drives

Internal SSD

Internal SSD

System Memory

8GB

8GB

16GB

Available Storage Capacity

1x 500GB

1-6x 3TB JBOD

1-4x 3TB JBOD w/DVD

1-6x 3TB RAID5

1x 500GB

1-5x 4TB JBOD*

1-4x 4TB JBOD w/DVD

3-6x 4TB RAID5

Monitor Connections

2x DVI-D:max resolution 1920x1200

 

1 VGA: max resolution: 1920x1200

 

1 DVI-D: max resolution:1920 x1200

 

2 Display Port

max resolution: 3840x2160

 

 

1 VGA

max resolution: 1920x1200

1 DVI-D: max resolution:1920 x1200

 

2 Display Port

max resolution: 3840x2160

 

 

1 VGA

max resolution: 1920x1200

 


 

* The internally mounted SSD occupies one of the six available SATA connections on the mother board, leaving 5 of the front panel drive trays available for storage drives.