From the Monitor (the main MPM), I can pick up values from other MPM, but the other MPM could not pick up values from the Monitor.

Issue

From the Monitor (DEV100) it is possible to pick up values from other MPMs, by the use of an LUA script.

Example:

ME.AV1 = DEV200.AV1

But, it is not possible for another device to pick up values from the Monitor (DEV100) device.

Product Line

SmartStruxure Lite

Environment

MPM

Cause

The Monitor device (DEV100) could see all other MPM in the network, and therefore could get values from other devices.

Other devices will only see devices that are below itself in the tree structure, and will therefore not be able to get values from the Monitor device.

Resolution

The Monitor device (DEV100) have to handle all the transfers of variables both from MPM below, as well as sending variables to MPM devices below in the tree structure.

Example:

ME.AV1 = DEV200.AV1
DEV200.AV2 = ME.AV2