How to switch camera display on a KBD300A connected to a DX4700/DX4800 series.

Issue

How to switch camera display on a KBD300A connected to a DX4700/DX4800 series.

Product Line

Pelco Video Management

Environment

  • KBD300A
  • KBD300USBKIT
  • DX4700 Series
  • DX4800 Series

Cause

Program information on how to switch camera display.

Resolution

  1. On the KBD300A Press the Shift Button and the Green LED will turn On.


     
  2. Press the F2 button (single screen).


     
  3. Verify Main monitor switches to single screen displays.
     
  4. Press the 1 button then the CAM button. (Number + Cam) 


     
  5. Repeat steps four to call up a different camera display.

    Note: Turn ON Shift key to Call Up or Switch the camera.  Shift key needs be OFF for the PTZ control.

Related articles:
How to connect the KBD300USBKit with the DX4700/DX4800 series DVR.

Is the KBD300A keyboard compatible with the DX4700/DX4800 Series hybrid video recorders (HVRs) and what are it's functions.