USRACK blank front panel plate.


  • What is the front panel blank off plate to the USRACK?
  • The USRACK has open spaces and I need the blanking plate please.
  • I have a USRACK for the newer fiber modules and I need to shut off the open spaces. What do you have to help with this?
  • What is the part number to the blanking plate?

Product Line

Pelco Transmission & Power




The USRACK module has empty slots and there is a need to close them off.


Use the paret number of RACK1B for the single-width blanking plate for the USRACK/EURACK assemblies.


This blanking plate looks like this: RACK1B plate.