Displaying a PDF file in a Niagara G3 / AX graphic.

Issue

Using 3.7.106 and want to display a PDF file on a Niagara G3 / AX graphic. It's been done in the past but with "Default Web Profile" "Applet Reload on Hyperlink" set to "False" the PDF does not display.

Is there a way to do it without setting the "Applet Reload on Hyperlink" to "True"?

 

Product Line

TAC I/A Series

Environment

Niagara G3 / AX revision 3.7.106 and higher

Cause

More secure changes made to G3 / AX

Resolution

Instead of creating a hyperlink button with hyperlink:  file:^blahblah.pdf

Use, http://137.19.60.55/ord?file:^blahblah.pdf

This opened the pdf in the browser (it left the default web profile but the back button returned to it).