Can the remote sensor with override switch (SE3020W1045) be interfaced to a SE7600H5045B and be accessed via a BACnet integration?

Issue

Can the remote sensor with override switch (SE3020W1045) be interfaced to a SE7600H5045B and be accessed via a BACnet integration?  The override switch is a trigger to provide cooling to the area served.

Product Line

SmartStruxure Lite

Environment

SmartStruxure Lite

Cause

Provide end user a simple way to get comfort coooling

Resolution

Interface the override switch to DI 01 on the SE7600H5045B.  It will then be accessible via BACnet to trigger comfort cooling.