What are the main differences between Continuum v1.94 SP1 and Continuum v2.0?

Issue

What are the main differences between Continuum v1.94 SP1 and Continuum v2.0?

Product Line

Andover Continuum

Environment

Continuum v2.0

Cause

Required a quick list of differences between the versions of Continuum to evaluate if a site upgrade to v2.0 was beneficial.

Resolution

The main features that Continuum v2.0 has over v1.94 are listed below.

  • Microsoft Internet Explorer 10 32 bit support
  • SQL Server 2012
  •  Microsoft Internet Explorer 11 32 bit support
  • Software licensing Support. See LL#13972.
  • Email SMTP Support. See LL#16848.
  • Extended Custom Wiegand Card* (ACX Series Only). See LL#17898.
  • Support for new door attribute 'ValidAttempt' see LL#18343 for more information.

 

You can also find more details in the v2.0 Feature Blast.

And further information on Continuum v2.0 with the links in LL#16713.