How to unlock the tilt screw on IS50 IS51 camclosure

Issue

Unable to get tilt to move

Product Line

Pelco Cameras

Environment

  • IS50 series
  • IS51 series

Cause

When shipped the camera tilt is locked by default with 2 screws.

Resolution

Looking at the front of the IS50/51 series camera you will see there is two screws one on each side pictured below.

 

 First you have to loosen the first screw until its almost out this is the shipping lock screw see pictured below 

 

Then loosen just a little the second screw and move your tilt to the desired position then tighten back up the second screw pictured below

 

 Note: You must loosen the first screw until its almost all the way out before you can adjust the tilt.