How to enable the motion detection service from Endura Utilities

Issue

Third party integrations such as exacqVision VMS fails to enable the camera's motion detection service.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Pelco Endura Utilities - Latest Version
  • Pelco Sarix Cameras
  • Pelco Camera API Integrations
  • 3rd Party VMS - Video Management Systems
     

Cause

Third party VMS fails to send the correct API call to enable the Pelco camera's motion detection service.

Resolution

How to enable the motion detection service from Endura Utilities.

1. Download and install Endura Utilities.  See Lessons Learned Article LL#8397 for the download link
2. Launch Endura Utilities
3. Click on the System Attributes tab
4. Click on the camera model from the left pane
5. Click on the specific camera from the right pane
6. Right Click and select Device Actions > Enable/disable motion service...



7. Choose Enable from the drop down menu then click OK