Can a Script Function be used in the Conversion line of a BACnet b3 controllers analog input?

Issue

If the conversion line on an input is more complex than a single line of script, can a function be used?

Product Line

SmartStruxure Solution

Environment

BACnet b3 Controller Analog input conversions / scaling.

Script programming, functions

Cause

The code required to scale an input is more complex than a single line of code.

Resolution

It is not possible to use a Script Function in the conversion line of an input point, however quite complex formulas can still be entered that scale the ElecValue when the point is evaluated.

The automatic scaling table is also available in the b3 inputs for linear conversions