Pelco's shock test conformity for impact ratings for domes and housings.

Issue

  • What shock obsorbancy does Pelco's lower domes handle?
  • Can Pelco's cameras stop a bullet?
  • Are Pelco's cameras bulletproof?
  • How much impact can a Vandal Resistant camera accept?
  • What does Pelco test against for shock rating?

Product Line

Pelco Cameras

Environment

All of Pelco's integrated domes and PTZ models along with enclosures with clear glass/lexan plastic as windows.

Cause

Unknown shock rating for certain sites and it is needing to be known if Pelco's cameras can fit into certain locations.

Resolution

Pelco's tests for shock ratings and impact ratings follow the IK10 impact rating standards.

More information about the IK rating scale is found here: EN62262 Standards.