Programming an 8-Bit Prox/Pin Pad Reader in I/Net Seven

Issue

Programming an 8-Bit HID or Indala Prox/Pin Pad reader

Product Line

TAC I/NET

Environment

I/Net Site with Access Control

Cause

There is a requirement to supply an 8-Bit Prox/Pin Pad reader at a site. How do I program this reader?

Resolution

Attached is a PDF File that guides you through the setup if this type of reader in an I/Net Seven system. Click here to download.