Monitoring an external variable outside of SmartStruxure Lite to trigger a lua script

Issue

At times it is necessary to monitor an external variable to trigger action in SmartStuxure Lite

Product Line

Andover Continuum, SmartStruxure Solution, SmartStruxure Lite

Environment

Smart Struxure Lite

Smart Struxure

Continuum

AS

MPM

Windows 7

Windows Server 2008

Cause

Need the ability to trigger actions from an external variable to run a lua script

Resolution

Use a lua script in your MPM that copies the value of ME.PG#_ENABLE.value to an Analog/binary value.

This value can then be seen from the AS or BCX through bacnet and you can have the AS or BCX do different functions depending on that value