Fail to add MNL controller in Workstation for Projects

Issue

When adding MNL controller in Workstation for Projects, it will show up an error: Object type is not supported.

Product Line

TAC I/A Series, SmartStruxure Solution

Environment

SmartStruxure 1.5

Workstation for Project

PCS

MNL controller

Cause

When using the Project Configuration Server, you cannot create MNL LonWorks devices and applications. Accordingly, the WorkPlace Tech Editor option does not display in the Control Panel.

Resolution

MNL LonWorks devices can be added in an Enterprise Server or Automation Server after deploying a project to one of these servers.