What is the part number for the upgrade/replacement hard drive on the DSSRV2?

Issue

What is the part number for the upgrade/replacement drive on the DSSRV2?

Product Line

Pelco Video Management

Environment

  • DSSRV2

Cause

Would like to purchase additional drives for the DSSRV2

Resolution

Replacement Hard Drives

  • 500GB HARD DRIVE = DSHDD-005
  • 4TB HARD DRIVE = DS-EN-HDD-4TB
  • 120GB HARD DRIVE = DS-EN-SSD-120GB

Both of these hard drive packages include the following items:

  • The respective hard drive of capacity listed.
  • HDD handling instructions.
  • Disposable antistatic wrist strap
  • Four phillips-head mounting screws

 

Upgrade Hard Drives

  • The 500GB and 4TB hard drive part numbers apply, however most systems would be updated using the 4TB drives
  • If expanding storage capacity af a RAID system, up to 6 hard drives may be used
  • If expanding the storage capacity of a JBOD system, the system will support up to 5 hard drives
  • All DSSRV2 platforms, whether RAID or JBOD, will have a maximum onboard storage capacity of 20TB

If a replacement drive tray is required, part number ZSPDSSRV-0001 may be used.

Please contact your Pelco dealer or distributor for pricing information or information regarding warranty replacement of HDDs and/or HDD trays.

 

For replacement hard drives for the 1st generation DSSRV NVR see:

Digital Sentry Network Video Recorder (DSSRV) replacement hard drives