How do I associate an analog audio contact to an IP camera connected to Digital Sentry?

Issue

How do I associate an analog audio contact to an IP camera connected to Digital Sentry?

Product Line

Pelco Cameras, Pelco Video Management

Environment

Digital Sentry Software

Cause

Application to record IP camera using an analog audio contact to associate with the IP camera.

Resolution

To Associate an Analog contact to an IP camera the Digital Sentry software version must be release 7.5.410 or Higher.

Open DS Admin and navigate to the IP camera.

Drop down the Associated Audio Channel and select the analog contact audio is wired to.. SAVE.