Unknown Exception when opening a project in Workstation for Projects

Issue

When opening a project in Workstation for Projects, Unkown Exception error will pop up

Product Line

SmartStruxure Solution

Environment

SmartStruxure 1.5

Workstation for Project

PCS

Cause

This is a defect for SmartStruxure 1.5. When there is no Internet connection on this computer, this error will happen.

Resolution

This issue will be fixed in SmartStruxure 1.6. Currently the workaround is to obtain the Internet connection for this computer, at least when opening the project. It should be OK to remove the Internet connection after the project is opened.