Does Helix YUV Codecs (remove only) application have anything to do with Continuum?

Issue

"Helix YUV Codecs (remove only)" shows up under Windows "add/remove programs" after Continuum is installed. Customer IT is questioning what this is and if it is part of Continuum.

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Windows

Cause

Codec is installed as part of the Continuum Cyberstation installation.

Resolution

Helix YUV Codecs is part of the Continuum installation. The installation file is "yuvcodecs-1.2.exe" located on the CD in "..\Continuum\ISSetupPrerequisites\{1D2652A6-D9B2-43ED-8009-987E762962A2}".