Alarm/Contact closure through Fiber.

Issue

  • Does Pelco have a fiber module with contact closure?
  • What fiber models give me a contact closure?
  • Does Pelco offer fiber products with alarming or contact closure?
  • Alarm or Contact closure fiber models?

Product Line

Pelco Transmission & Power

Environment

Fiber - FTV10D1A2 and FRV10D1A2 ONLY

Cause

Difficulty in obtaining the one model series of fiber products that have the single contact closure option.

Resolution

The only option that Pelco has to offer, with regards to contact closure within fiber optics solutions is the FTV10D1A2 and FRV10D1A2 pair. The Spec Sheet for this product can be found in the link provided.

There is NO In-Camera fiber card option that provides contact closure. So, in this instance, the FS85011A and/or the FSV10D1 fiber modules will NOT work with contact closure.