The DX4500/DX4600 is display Out of Range on the main monitor output.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

There is no mouse control or live video on the main monitor output.

Product Line

Pelco Monitors, Pelco Video Management

Environment

  • DX4500 Series
  • DX4600 Series
  • Monitor

Cause

  • A power surge causing the monitor output on the DX45/4600 to switch.

Resolution

Switch the monitor output back to main vga on DX4500.
 

VGA Output: 
On the front panel press and Hold the MAIN button. After approximately five seconds the system will beep and restart. Verify the main video display on the VGA monitor.


 

.