DSSRV2 installation

Issue

DSSRV2 connection installation.

DSSRV2 Default Login

Product Line

Pelco Cameras, Pelco Monitors, Pelco Video Management

Environment

  • DSSRV2
  • DSSRV2-Raid
  • ENC5516
  • ENC5400-4PORT

Cause

DSSRV2 hardware connection information

Resolution

  1. With the power off on the DSSRV2 make all necessary connection.(Monitor, mouse, keyboard,network)
    Note: Display port to DVI single-Link must be a Active converter for the two DP monitor outputs.


    Note: The Interface RJ-45 Gigabit Ethernet Ports (1000Base-T)  are non load balancing. It is recommended that the DSSRV use a Gigabit connection (link speed) per NIC.
    Note: The Interface RJ-45 Gigabit Ethernet Ports (1000Base-T)  are non load balancing. It is recommended that the DSSRV use a Gigabit connection (link speed) per NIC.
    Note: The Interface RJ-45 Gigabit Ethernet Ports (1000Base-T)  are non load balancing. It is recommended that the DSSRV use a Gigabit connection (link speed) per NIC.
    Note: The Interface RJ-45 Gigabit Ethernet Ports (1000Base-T)  are non load balancing. It is recommended that the DSSRV use a Gigabit connection (link speed) per NIC.
    Note: The Interface RJ-45 Gigabit Ethernet Ports (1000Base-T)  are non load balancing. It is recommended that the DSSRV2 use a Gigabit connection (link speed) per NIC.
     

     
  2. With the power off connect ENC5516 to the ENC5400-4PORT.


    DSSRV2-Raid/ENC5400-4PORT install diagram . Note: Install in slot PCIE X16.



    ENC5400-4PORT card



     
  3. Turn on the ENC5516
  4. Turn on the DSSRV2.
  5. Log into windows when prompt. (default User name:DSServiceUser, Password: dsserviceuser)
  6. Name the compter and enter the static ip address using network and sharing  center. refer to article LL#14285 
  7. Then reboot system. Then log back into windows
  8. Run DS quicksetup for 1st time setup.
     

Related articles:
Which network interface is used on the DSSRV (Digital Sentry)
Using DS Quick Setup to configure both new and existing setups for the Digital Sentry Software Suite.
Configuring Digital Sentry software suite using DS Admin.
Comparison Between DSSRV, DSSRV2, DSSRV2-RD
How to setup the DSSRV to support Coaxitron PTZ control with the ENC5516.