Unable to set a preset On Spectra Pro PTZ if it uses the characters #,%, &, also cannot delete the name out of the list

Issue

If you use the characters "#,%, &",  you cannot set the preset and you will not be able to delete it from the list, these are not valid characters for a preset name.

Product Line

Pelco Cameras, Pelco Video Management

Environment

Spectra Pro PTZ while making presets

Cause

The #, % and & are not considered valid characters to the preset program

Resolution

DO NOT use these characters, at this time these cannot be deleted from the preset list