What slot should the ENC5400-4PORT and RAID card use on the DSSRV2 motherboard.

Issue

What slot should the ENC5400-4PORT and RAID card use on the DSSRV2 motherboard.

Product Line

Pelco Video Management

Environment

  • DSSRV2-RAID
  • ENC5400-4Port

Cause

Installing the LSI 3Ware9750-8i RAID controller card into the correct slot.

Resolution

Install the DSSRV2-RAID card into the first PCIe-16X slot.  If an ENC5400-4 Port card is installed, it will go into the 2nd PCIe-16x slot and the DSSRV-RAID card to be installed into the PCIe-16x slot closest to the processor.   

 

 

SSD Connection