The status of a Forced BACnet value is not reflected in a Graphic or the Watch Window.

Issue

The status of a Forced BACnet value is not reflected in a Graphic or the Watch Window.

Product Line

SmartStruxure Solution

Environment

ES, AS

Cause

Function as designed.

Resolution

It was designed so that the "Forced" status for BACnet values would not be displayed in graphics or the watch window.

For a workaround using a PE Script program to show the forced icon for a BACnet value see http://buildingskb.schneider-electric.com/view.php?AID=17876