How do I adjust the Dwell on the VS5104

Issue

Sequence dwell times require adjustment

Product Line

Pelco Matrix

Environment

  • VS5104
  • VS5108

Cause

Installation and Service

Resolution

Adjust the DWELL interval control with a screwdriver to the desired switching interval, 1 to 70 seconds nominal. Rotate the control pot clockwise for longer intervals and counter-clockwise for shorter intervals. This control pot is a 15-turn precision potentiometer. The approximate ratio is one full turn is equal to 4–5 seconds of delay.