How to playback .exp video files from a DX4700_DX4800 server.

Issue

How to playback .exp video files from a DX4700_DX4800 server.

Product Line

Pelco Video Management

Environment

  • DX4700nonHD
  • DX4700nonHD
  • DX4700HD
  • DX4800HD
  • .EXP video export

Cause

DX4700/DX4800 server allows you to play back .exp video export.

Resolution

The Export Review search feature allows you to search video exported to USB or CD/DVD media

  • The unit supports the play , pause , and stop buttons when playing back exported video. The reverse start, reverse, fast
    forward, end playback controls are not supported.
  • When playing back exported video on the USB device, paused video will jump forward in time when playback is resumed.

To conduct an export search:

  1. Click on the search from the tool bar menu.


     
  2. From the Search menu, click Export Review.


     
  3. Select a media.
  4. Click Search. The search results appear.
  5. Select an entry, and then click Play. Video is played back in the 1 x 1 view.


     
  6. Click the Stop icon  to stop playback.