DS ControlPoint 7.7 and above does not allow the 6x6 (36) screen layout in Full Screen view.


DS ControlPoint 7.7.309 no longer has the 6x6 (36) screen layout option available with "Full Screen"  view.

Product Line

Pelco Video Management


  • DS ControlPoint 7.7.309
  • Digital Sentry
  • 36 camera display layout - Full Screen


The Full Screen option has been removed from DS ControlPoint 7.7.309 and above when using a 6x6 layout to resolve a software problem.


DS ControlPoint starting with version 7.7.309 and above will no longer offer the 6x6 (36 camera) screen layout in Full Screen mode, this has been done to resolve other software issues caused by this layout.

All other layouts will have the "Full Screen"  option available. Recommend using the 5x5 layout if maximizing camera count with the Full Screen option is desired.