FD2 Camera Adjustment

Issue

Ability to invert or adjust the viewing angle of the FD2 camera when mounting on a wall instead of a ceiling.

Product Line

Pelco Cameras

Environment

FD2 series

Cause

When mounting the FD2 on a wall instead of ceiling mount, camera view is upside down or sideways.

Resolution

The viewing angle of the FD2 can be manipulated to compensate for various mounting configurations. To accomplish this task perform the following steps:

  • Remove the Dome cover
  • Remove the Inner liner   

Once this is accomplished, manipulation of the camera is done in the following manner:

  •  Rotate 3D assembly in base for pan adjustment
  •  Tilt adjustment bracket and screw for vertical adjustment
  •  Axis ring for horizontal rotation for wall mount and tilted ceilings