Displaying Video on the Main and Spot monitors on a DX4700_DX4800 Series.

Issue

Unable to change the video display on a DX4700 main output.

Product Line

Pelco Video Management

Environment

  • DX4700
  • DX4800
  • DX4700HD
  • DX4800HD

Cause

User unfamiliar with DX4700_DX4800 Series.

Resolution

Main Monitor

To display video from one channel in the single view mode, double-click a pane. To display video from all channels in individual panes, double-click a pane.

To select a division:
 

  1. Click the Main  monitor icon
     
  2. Click a division            
                                 

     
  3. Click OK



To view channels in the sequence mode:
 

  1. Click the Main monitor icon
     
  2. Click the Sequence   button
     
  3. Click division
     
  4. Click OK

 

SPOT MONITOR

The Spot monitor allows you to monitor video on a single or quad division

To select a division:

  1. Click the Spot monitor icon
     
  2. Click a division


     
  3. Click OK


To view all channels in the sequence mode:
 

  1. Click the Main monitor button
  2. Click the Sequence  button
     
  3. Click a division
     
  4. Click OK