Which versions of SIGNAL can be migrated to SBO?

Issue

Which versions of SIGNAL can be migrated to SBO?

Product Line

TAC I/A Series, SmartStruxure Solution

Environment

SIGNAL

Cause

The migration manual does not identify which versions are accepted.

Resolution

Two versions of SIGNAL can be backed up and migrated to SBO:  Version 4.4.1 (for Windows 95/98) and Version 5.0.0 (for Windows XP).