Replacement actuator for TAC AF24-SR

Issue

TAC AF24-SR is obsolete and needs to be replaced.

Product Line

Field Devices

Environment

TAC AF24-SR

Cause

Replacement of obsolete actuator. 

Resolution

The TAC AF24-SR damper actuator is replaced by the MD10SR or MD20SR actuators – in the USA it is also possible to use the MS41 actuators

 
 
replaced by the MD10SR or MD20SR actuators – in the US they would make this cross but we do not really sell the US MS41 actuators
 
replaced by the MD10SR or MD20SR actuators – in the US they would make this cross but we do not really sell the US MS41 actuators