Is the FMCI-PF1 compatible with a FMCI-PG1?

Issue

The manuals do not state that the FMCI-PG1 and the FMCI-PF1 are not compatible. They are not

Product Line

Pelco Cameras, Pelco Video Management, Pelco Transmission & Power

Environment

When trying to use an FMCI-PG1 with a FMCI-PF1

Cause

These two unit types run at different speeds and are not compatible

Resolution

You must use a FMCI-PG1 with a FMCI-PG1 and the same with an FMCI-PF1. It has to be used with a FMCI-PF1