Error : database cannot be accessed you may be in single user mode NS #22

Issue

NL220 Data base will not open and an Error, "database cannot be accessed you may be in single user mode NS #22" is produced.
 

Product Line

TAC Vista

Environment

LNS

LonMaker

Vista

NL220
 

Cause

Administration rights are not granted to the microsoft server computer user, preventing the database from opening.

 

Resolution

To work around admin access from IT, close Nl220 and right click re-launch using "run as administrator".