How to turn off Pan or Tilt Limits on Esprit cameras


Camera tilts or pans during a preset or pattern, but when manipulated with a joystick it gives an error message of pan or tilt limit

Product Line

Pelco Cameras


Esprit series cameras


Limit Stops have been programmed


To eliminate the error and restore proper function, perform the following steps:

  1.  Program preset 95 (28 if older model), main menu should appear.
  2.  Position the cursor (>) beside Limit Stop.
  3.  Press the Iris Open button to enter the Limit Stop menu.
  4.  Move the cursor to Clear Scan Limits and press the Iris Open button.  NOTE: The cursor will flash to an asterisk (*) briefly to indicate the limits have been disabled.