How do I Import or export System configurations on the DX4500/ DX4600 DVR

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

The DX4500/DX4600 Configuration option allows you to import and export the DVR configuration settings.

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600 Series

Cause

  • Installation and Service
  • Multiple DVRs can be configured quickly from a USB drive. Factory defaults can be easily restored.

Resolution

From the System menu, on the front panel or remote control, press ENTER. Then press the up/down arrow buttons to highlight Configuration. Using the mouse, click the Configuration option. The Configuration settings are displayed.

 

To import configuration settings:

a. Insert the USB device.

b. On the front panel or remote control, press ENTER twice. Using the mouse, click the Selection settings box. The “Would You Like to Import the Configuration?” dialog box opens.

c. On the front panel or remote control, press the left/right arrow buttons to highlight OK, and then press ENTER. Using the mouse, click OK. The import process starts. After the import process is complete, the “Configuration Import Complete” dialog box opens.

d. On the front panel or remote control, press the left/right arrow buttons to highlight OK, and then press ENTER. Using the mouse, click OK.

To export the DVR configuration settings:

a. On the front panel or remote control, press the up/down arrow buttons to highlight Configuration Export, and then press ENTER. Using the mouse, click the Configuration Export settings box. The “Would You Like to Export the Configuration?” dialog box opens.

b. On the front panel or remote control, press the left/right arrow buttons to highlight OK, and then press ENTER. Using the mouse, click OK. After export process is finished, the Configuration Export Complete dialog box opens.

c. On the front panel or remote control, press the left/right arrow buttons to highlight OK, and then press ENTER. Using the mouse, click OK.