Which Pelco IP cameras and encoders are ONVIF compliant?

Issue

ONVIF information regarding Pelco IP cameras and Encoders.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Sarix
  • Sarix with SureVision
  • Sarix TI
  • Spectra IV IP H.264
  • Spectra HD
NET5400Sarix, Sarix with SureVision, Sarix TI, Spectra(r) IV IP, Spectra HD, and NET5400All models of Sarix,S Sarix with SureVision,s Sarix TI, Spectra(r) IV IP,
Spectra HD, and NET5400 Series encoders now conform to the ONVIF 1.02
standard as of firmware version 1.8.2.

Cause

Pelco cameras that conform to ONVIF standards are unclear or unknown. 

Resolution

All models of Sarix, Sarix with SureVision, Sarix TI, Spectra(r) IV IP H.264, Spectra HD, and NET5400 Series encoders now conform to the ONVIF 1.02 standard as of firmware version 1.8.2.