How do I stop a Macro using the KBD960 Keyboard

Issue

A macro is a sequence of commands or steps. When you run a macro, the steps programmed into that macro are performed. Macros can be run manually or automatically. Automatic operation can be the result of alarms or the reaching of specific times and dates.

Product Line

Pelco Matrix

Environment

  • KBD960
  • CM6800 Matrix Switcher

Cause

A continuous macro runs until you clear it or stop it.

Resolution