Is there a Display Port to DVI adapter for the DSSRV2?

Issue

Would like more than one VGA or DVI connection to the DSSRV2 and does not have Display Port compatibility for their monitor outputs.

Product Line

Pelco Video Management

Environment

  • DSSRV2
  • Display Port (DP) adapter

Cause

No Display Port to DVI adapter included with the DSSRV2 literature kit. 

Resolution

There is a Display Port to DVI adapter that is currently included with the DS-CPPC-LIT and WS5080-LIT-KIT literature kit part numbers.

The part number for this adapter is CN17-8221-1001G.

  • Converter Type: Active
  • Maximum Digital resolution: 1920x1200