EH3010 and EH3014 enclosures have been set to OBS Immediately

Issue

The  EH3010 and EH3014 series have gone OBSOLETE

Product Line

Pelco Cameras

Environment

 

EH3010

Indoor Extruded aluminum enclosure, 11.50-inch (29.21 cm) length

 

EH3014

Indoor extruded aluminum enclosure, 15.50-inch (39.37 cm) length

 

Cause

Due to a current global shortage of an important component, we are not able to build the enclosures. Additionally, our Service and Repair department will support EH3010 and EH3014 through the warranty, which is one year after date of purchase

Resolution

Please contact your regional sales for any replacement options